SOFTWARE DOWNLOAD

Software upgrade

In this section, it is possible to download the most recent revisions of the LOVATO Electric PC software. These upgrades are available exclusively to users that have already installed a previous revision of the software from an original LOVATO Electric CD.

  • It is recommended to make a backup copy of the original files.

  • Click on the required upgrade, fill in the form with your data and then click on the Download button.

  • Select 'Save file on disk' option and wait for the download.

  • Extract the new files from the downloaded .zip file, specifying destination directory as the one used for the installation of the original software.

  • Read additional instructions given in the UpgradeNotes.txt file.



Metering instruments and current transformers

Soft starters

Automatic power factor controllers

Automatic transfer switch controllers

Engine and generators controllers
RGAM10, RGAM12/24, RGAM20, RGAM4..., RGK20, RGK40, RGK50, RGK60, RGK700, RGK800

 

LEGAL NOTICE
The products described in this site are subject to be revised or improved at any moment. 
Descriptions and details, such as technical and operational data, drawings, diagrams and instructions, do not have any contractual value.
In addition, products must be installed and used by qualified personnel and in compliance with the regulations in force for electrical systems in order to avoid damages and safety hazards.
Any software downloaded from this site constitutes the copyrighted work of LOVATO Electric.
Any software reproduction, copying, distribution or retransmission by the user is expressly prohibited by law. The use of the software for any other purpose than with the specifically designed products is also prohibited and is solely for the user's own application. 
The user is fully responsible for the software and the hardware products thereby associated.
LOVATO Electric disclaims all responsibility related to loss of and incidental, consequential or indirect damage to programs or data as well as damage deriving from improper use of the software or user's negligence.

 

     
HOME PAGE
LOVATO Electric S.P.A.